CONNECT-Output
CONNECT associates a given control or sensor with a pin or port on the TI-Innovator. If the specified control or sensor is currently in use, an error will be generated. If the pin or port specified in the CONNECT command is currently in use, an error will be generated.
The CONNECT command does not generate an active response, but a variety of errors may occur during a connection attempt, such as pin-in-use, unsupported, invalid options, bad options, etc.
CONNECT 'something i' [TO] IN1/IN2/IN3/OUT1/OUT2/OUT3/BB1
|
Command: |
CONNECT |
|---|---|
|
Command Syntax: |
CONNECT |
|
Range: |
|
|
Describe: |
Associates a sensor or control with a given port or pin(s). Places the respective pin(s) in use |
|
Result: |
|
|
Type or |
|
Commands for CONNECT-Output
|
|
CE Calculators
|
TI‑Nspire™ CX
|