VERNIER

Command:

CONNECT VERNIER i TO IN n

Command Syntax:

CONNECT VERNIER 1 TO IN 1 AS LIGHT

CONNECT VERNIER 2 TO IN 2 AS ACCEL

CONNECT VERNIER 1 TO IN 1 AS ENERGY

Range

Describe:

This command is used when a Vernier analog sensor is connected to the TI-Innovator™ Hub through the TI-SensorLink

There is support for three additional Vernier analog sensors

• LS-BTA
• LGA-BTA
• VES-BTA

Result:

 

Type or
Addressable Component:

Sensor