15.5
unpack
..., remnant = string.unpack("formatString", characteristicValue)
Unpacks a Bluetooth ® LE characteristic data value into one or multiple Lua values. The number of returned values is defined by the format specifiers inside the formatString. All supported format specifiers are listed in Table 1.3 and additional details can be found in subsection 20.1.5 .
|
Parameter |
Type |
Description |
|---|---|---|
|
"formatString" |
in string |
Lists one or multiple formats to be unpacked |
|
characteristicValue |
in string |
The characteristic value read. |
|
... |
out any |
The parameter list associated to the format specified |
|
remnant |
out string |
The remnant of the characteristicValue if the format did not decode all data, or nil otherwise. |
Listing 1.21: Example Showing the use of string.unpack()
bool1, number, bool2 = string.unpack("bb2b", data)
bool1, bool2, bool3 = string.unpack("bbr2b", data)
Similar to the pack function it is possible to split the unpacking of the data into multiple calls to unpack. This can be achieved by passing the remnant returned of one call to unpack as characteristic value to the next call of unpack. Listing 1.22 show the two scenarios.
Listing 1.22: Splitting Unpacking into Multiple calls to string.unpack()
ten, twelve = string.unpack('u8u8', '\\10\\12')
ten, remnant = string.unpack('u8', '\\10\\12') -- returns 10, '\\12'
twelve = string.unpack('u8', remnant) -- returns 12, nil
Introduced in platform.apiLevel = '2.7'