21.5 startScanning

error = asi.startScanning(portFoundCallback [, object])

Scans for ASI ports. A second call to startScanning while already scanning does not reset the process. If a rescan is desired, call stopScanning first and then startScanning to reset the process.

Parameter

Type

Description

portFoundCallback

in function

Callback to receive ports found, one call per port.

object

in any (optional)

If an object is provided, it will be passed as the first parameter to the specified callback function.

The object can be of any type except nil.

error

out string (optional)

If successful nil is returned, an error message otherwise.

Introduced in platform.apiLevel = '2.7'.

Callback Function

portFoundCallback ([object,] port)

The callback function provided in startScanning will be called for every ASI port found. The port parameter will be a port object representing the port interface found. One call per port found. Ports maybe present at the moment of calling asi.startScanning() or later added while scanning. Ports are reported only once between startScanning/stopScanning cycles.

Parameter

Type

Description

object

in any
(optional)

If an object was provided as a parameter to the function startScanning, it will be passed as the first parameter to this callback function.

port

in port object

One port found during scanning.

Introduced in platform.apiLevel = '2.7'.