8.44 varChange

on.varChange(varlist)

This routine is called when a monitored variable is changed by another application. The varlist is a list of variable names whose values were changed. This handler must return a value to indicate if it accepts the new value(s) or vetoes the change.

Valid return values are:

Value

Brief Description

Comment

0

Success

The script application accepts the change.

-1

Veto range

The new value is unsatisfactory because it is outside the acceptable range, which is too low or too high.

-2

Veto type

The new value is unsatisfactory because its type cannot be used by the script application.

-3

Veto existence

Another application deleted the variable, and this application needs it.

Introduced in platform.apiLevel = '1.0'