Arranging the Seating Chart
Initially, students are arranged in the Seating Chart view in the order that you added them. However, you can rearrange the students so that they have the same seating arrangement in the Class Workspace as they do in your actual classroom. You can rearrange the seating chart at any time.
Arranging Students in the Seating Chart
| 1. | Select the class from the Class Session list. |
| 2. | Click View > Seating Chart. |
The classroom area shows your class in the Seating Chart view.
| 3. | Within the classroom area, drag each student icon to the location that you want. |
The software moves the student icons to the new locations.
The software remembers the student positions the next time you start the same class.
Note: Do not place one student icon on top of another student icon. If you do this, you will only be able to see one of the student’s icons.