Installing a Python program as a module

To save your Python program as a module:

• In the Editor, select Actions > Install as Python Module.
• In the Shell, select Tools > Install as Python Module.

After selection, the following occurs:

• The Python syntax is checked.
• The file is saved and moved to the PyLib folder.
• A dialog appears confirming that the file has been installed as a module.
• The file is closed and the module is ready for use.
• The module name will be added to the More Modules menu with a from <module> import * menu item.

If you plan to share this module with others, it is recommended that you follow these guidelines:

• Store only one module per TNS file.
• The module name matches the name of TNS file (e.g. "my_program" module is in the "my_program.tns" file).
• Add a Notes page before the Python Editor that describes the intent of the module, the version, and the functions.
• Use the ver() function to display the version number of the module.
• (Optional) Add a help function to display the list of methods in the function.