Viewing a Program or Function
| 1. | From the Actions menu, click View. |
| 2. | If the function or program is a library object, select its library from the Location list. |
| 3. | Select the function or program name from the Name list. |
The function or program is displayed in a viewer.
| 4. | Use the arrow keys to view the function or program. |
| 5. | If you want to edit the program, click Edit. |
Handheld: Press e to highlight Edit, and then press ·.
Note: The Edit selection is available only for functions and programs defined in the current problem. To edit a library object, you must first open its library document.