Exploring the Script Editor Interface

The Script Editor window opens when you insert a new script application or edit an existing script application in a TI-Nspire™ document.

Select options for creating new scripts or editing scripts from the Insert menu in the Documents Workspace when a document is open.

Note: Although not labeled, the Documents Workspace is the default workspace in the TI-Nspire™ CX Student Software and TI-Nspire™ CX CAS Student Software.

The following figure shows the Script Editor with an existing script.

 

Menu bar. Contains options for working with the Script Editor.

Toolbar. Provides tools for common Script Editor functions. See Using the Toolbar.

Script title. Shows script title. Right-click the title to change it or by clicking Edit > Set Script Title.

Text box. Provides a space to type script text.

Tools panel. Shows script data. See Using the Tools Panel.

Status bar. Displays the operational state of the script. See Using the Status Bar.