Setting Up the TI Bluetooth® Adapter and a Dash Robot for CE

CE Classroom Scenario

Materials Needed to Setup Dash Robot

At least one set* consisting of
Wonder Workshop Dash robot
TI Bluetooth® Adapter
One CE Calculator with
Latest CE Bundle
education.ti.com/84ceupdate
SetDash App
Download the App file from education.ti.com/dash
Send to CE calculator using TI Connect™ CE.
Suggestion:
Use small name labels on a robot/Adapter setup to keep your classroom sets of robots and Adapters organized.

 

*Note:

To perform the one time setup of your class set of robots and Adapters, setup one Dash robot, powered on, with one TI Bluetooth® Adapter at a time using the SetDash App running on your CE calculator.
While several Dash robots can be turned on in the range of a TI Bluetooth® Adapter, consider turning on one robot at a time for fast and efficient setup of this hardware set for your classroom.
The setup is a one-time effort since the TI Bluetooth® Adapter stores the specified Dash robot by the name and color you set.
When a group of students are sharing one robot and one Adapter, they can each write a CE Python program on their calculator. To run their own program from the CE Python App,
detached the shared Adapter from one CE
attached Adapter to another CE from the Python App
Run their Python program to watch Dash in action