Correcting an Error
To correct an error, follow these steps.
| 1. | Note the error type (ERROR:error type). |
| 2. | Select 2:Goto (if it is available).The previous screen is displayed with the cursor at or near the error location. |
| 3. | Determine the error. The error screens give helpful hints about what may have happened, but the errors are not always fully explained. |
| 4. | Correct the expression. |