STAT WIZARDS: ON OFF
ON: Selection of menu items in MATH PROB, STAT, CALC, DISTR DISTR, DISTR DRAW and seq( in LIST OPS displays a screen which provides syntax help (wizard) for the entry of required and optional arguments into the command or function. The function or command will paste the entered arguments to the Home Screen history or to most other locations where the cursor is available for input. Some calculations will compute directly from the wizard. If a command or function is accessed from N the command or function will paste without wizard support.
If no wizard is available, use Catalog Help for more syntax help when needed. To use Catalog Help, select a menu item and then press Ã.
OFF: The function or command will paste to the cursor location with no syntax help (wizard).