Setting Up Test Mode

1. Turn the calculator OFF.
2. Press and hold down the ~, | and É keys, and then release.
3. The RESET OPTIONS screen displays.
4. To change the default settings, move the cursor over the desired setting and press [enter].

By default:

• ANGLE is set to DEGREE
• STAT DIAGNOSTICS is set to ON
• DISABLE logBASE and DISABLE S( are set to YES
• DISABLE Numeric Solver is set to NO
5. Press OK to first validate any loaded TI Apps and then set up the exam mode. When validation and test mode setup is complete, the confirmation screen will display.

6. Press any key to place the calculator in test mode.

Note:

• The status bar is blue when in TEST MODE and TEST MODE ENABLED.
• Pic & Image Vars are disabled.
• All variables stored in RAM and in archived memory are deleted.
7. On the exam calculator, press Œ to verify that applications are disabled. The following screen displays:

8. On the exam calculator, press ¼ to verify that programs have been disabled. The following screen displays:

9. On the exam calculator, Pic and Image Vars are shown as disabled. The following screen displays:

10. In memory management (y L, 2:Mem Management/Delete...), disabled files will display with the not equal sign.