Using the TVM Variables

FINANCE VARS Menu

To display the FINANCE VARS menu, press Œ [enter] ~. You can use TVM variables in TVM functions and store values to them on the home screen.

CALC VARS

1: Ú

Total number of payment periods

2: æ

Annual interest rate

3: PV

Present value

4: PMT

Payment amount

5: FV

Future value

6: P/Y

Number of payment periods per year

7: C/Y

Number of compounding periods/year

N, I%, PV, PMT, FV

Ú, æ, PV, PMT, and FV are the five TVM variables. They represent the elements of common financial transactions, as described in the table above. æ is an annual interest rate that is converted to a per-period rate based on the values of P/Y and C/Y.

P/Y and C/Y

P/Y is the number of payment periods per year in a financial transaction.

C/Y is the number of compounding periods per year in the same transaction.

When you store a value to P/Y, the value for C/Y automatically changes to the same value. To store a unique value to C/Y, you must store the value to C/Y after you have stored a value to P/Y.