Menus and Functions
| • | To quit the App, select the QUIT-APP option at the upper-right of the Y=screen. Select 2:Quit Inequal at the prompt. |
| • | Inequality Graphing App and Transformation Graphing App cannot run at the same time since they enhance the Function Mode of the o editor. If the Apps are in conflict, follow the prompts to quit the conflicting App, which will allow the other App to run as an enhanced o editor. |
|
Menus |
Functions |
|---|---|
|
Graph/Plot Setup Keys |
|
|
Y= |
Displays the Y= Editor, where you can enter one or more inequalities to graph and change the graph color and line style. |
|
X= |
Graph a vertical inequality. |
|
Window |
Set the viewing window to produce the best display of your graph. |
|
Zoom |
Quickly adjust the window to a pre-defined setting. |
|
Trace |
Move the cursor along the graphed function using | and ~. |
|
Graph |
Display the graph you have defined.. |
|
Inequality Menu |
|
|
INEQUALITY |
|
|
1: Point of Interest Trace |
Trace points of interest (such as intersections) b.etween relations. |
|
2: Inequal Intersection |
Display the intersection of the inequalities and select the color of the shading. |
|
3: Union |
Display the combined area of the inequalities and select the color of the shading. |
|
4: Original ShadeRes= |
Return to the original inequality graph. |
|
5: Inequality App Help |
Help for Inequality Graphing. |
|
Quit Menu |
|
|
1: Continue Running |
Continue using the Inequality Graphing app. |
|
2: Quit |
Quit the App. |
|
3: About |
Display the opening screen with version number information. |