S
|
|
|||||||||
|---|---|---|---|---|---|---|---|---|---|
|
Module: ti_plotlib Syntax: plt.scatter(xlist,ylist,"mark") Description: A sequence of ordered pair from (xlist,ylist) will be plotted with mark style specified. The line style and size are set using plt.pen(). xlist and ylist must be real floats and lists must bee the same dimension. Argument: "mark" is the mark character as follows:
Example: See sample program: LINREGR. |
|
|
|
|
|---|---|
|
Syntax:
Description: Initialize random number generator. Example:
Results will vary given a random output. |
» Modul [Fns…] > Modul
y N
import commands can be found in |
|
|
|
|---|---|
|
Module: Built-in Syntax: set(sequence) Description: Returns a sequence as a set. See Python documentation for more details. Example:
|
|
|
|
|
|---|---|
|
Module: ti_plotlib Syntax: plt.show_plot() display > [clear] Description: Executes the display of the plot as set up in the program.
For plotting template help, from File Manager, select After running the program, the plotting display is cleared by pressing Example: |
[Fns…]>Modul or [math]
|
|
|
|
|---|---|
|
Syntax:
Description: Returns sine of Example:
|
˜ 3:sin()
y N
[Fns…] > Modul 1:math… > Trig 3:sin()
import commands can be found in |
|
|
|
|---|---|
|
Module: ti_system; time Syntax: sleep(seconds) Description: Sleep for a given number of seconds. Seconds argument is a float. Example: Sample program:
Run the program TIME
|
[Fns…]>Modul or » [Fns…]>Modul or »
|
|
|
|
|---|---|
|
Syntax:
Description: The method sorts a list in place. See Python documentation for more details. Example:
|
y 9 y N [Fns…] >
|
|
|
|
|---|---|
|
Syntax:
Description: Returns a sorted list from sequence. Example:
|
y 9 (above …) List
y N
[Fns…] > List |
|
|
|
|---|---|
|
Module: Built-in Syntax:var.split(x) Description: Method returns a list by specified separator. See Python documentation for more details. Example:
|
|
|
|
|
|---|---|
|
Syntax:
Description: Returns square root of Example:
|
» Modul 1:math 3:sqrt()
y N
[Fns…] > Modul 1:math 3:sqrt()
import commands can be found in |
|
|
|||||||
|---|---|---|---|---|---|---|---|
|
Module: ti_system Syntax: store_list("name",var) 1-6 Description: Stores a list from the execution of a Python script to an OS list variable "name" where var is a defined Python list. List length must be less than or equal to 100. Argument: "name" For OS L1-L6
For OS custom list "name" ----- Max 5 characters, numbers or letters, starting with letters, and letters must be uppercase. Examples: "ABCDE" "R12" "L1" will be custom L1 and not OS L1 Reminder: Python is double precision which is more digits than supported in the OS. Example:
Quit the Pyton App and press yd (above [ 1 ]) and [enter] on the Home Screen to see list d as {1 2 3}. |
yK
|
|
|
|
|---|---|
|
Syntax:
Description: Converts "argument" to a string. Example:
|
y N
[Fns…]
|
|
|
|
|---|---|
|
Syntax:
Description: Returns the sum of the items in a sequence. Example:
|
y 9 (above …) List
y N
[Fns…] > List |