The Python Experience

Using TI-SmartView™ CE-T to Demonstrate the Python Experience

Update to the latest TI-SmartView™ CE-T at education.ti.com/84cetupdate.
Launch TI-SmartView™ CE-T.
Run the Python App on the
TI-84 Plus CE-T emulator.
The Python App offers
File Manager
Editor
Execution of your Python program in the Shell
Add-On modules ti_draw and ti_image are also included.
SmartPad CE App will remotely press the keypad when the Python App is running.
You can send your computer *.py files to the Emulator Explorer workspace to convert your programs to PY AppVars.

Hub/Rover Programs

Create ti_hub/ti_rover Python programs in the CE-T emulator running the Python App.

*Note: There is no connectivity between TI-SmartView™ CE-T and TI-Innovator™ Hub or TI-Innovator™ Rover. Programs can be created and then run on the CE-T calculator.

Quit the Python App to prepare to transfer the Python AppVar(s) from the emulator. The emulator should not “be busy” running an App or program for the next step.
Change to the Emulator Explorer workspace and send the program(s) to the computer.
Use TI Connect™ CE to send the Python AppVars from the computer to the CE calculator for the TI-Innovator™ Hub/TI-Innovator™ Rover experience.

Note: To break a running Python program in the Shell, such as if a program is in a continuous loop, press [on]. Press [Tools] [zoom] > 6:New Shell as an alternate method to halt a running program.

Reminder: For any computer/TI-Python experience: After creating a Python program in a Python development environment on the computer, please validate your program runs on the calculator/emulator in the TI-Python experience. Modify the program as needed.

SmartPad CE App Remote Keypad

Running the SmartPad CE App on your connected CE-T functions as a remote keypad including the special keypad mapping offered when the Python App is running.

Emulator Workspace

- The CE emulator runs the Python App. To launch the Python App, select [prgm] 2:Python App. See: Programming Python in TI-84 Plus CE-T Python eGuide.

Emulator Explorer Workspace

Please quit the Python App so the emulator is not busy when you access the full features of the Emulator Explorer workspace.
- A Python program (PY AppVar) will save from the CE to a computer as *.py file. Open the *.py file in a text editor to view or edit the file for the CE Python experience. As in previous releases, TI-SmartView™ CE and TI Connect™ CE Explorer will send/convert *.py files to the calculator file type, PY AppVar. There is no need to save the CE PY AppVar on your computer.
- When sending an image from a computer to a connected CE, an additional image conversion option is available to convert and send the correct Python image AppVar format to the CE. Then, using the Python App, import the ti_image Add-On module to use the image in your program.

See: TI-84 Plus CE-T Python eGuide for details on TI-Python.

See: TI Connect™ CE eGuide for more details on image conversions.

When sending a program.py file created in another Python environment, your PY AppVar will need to be edited to run as expected in TI-Python. Use the Python App Editor to modify as needed for the unique modules such as
ti_plotlib, ti_system, ti_hub and ti_rover.

Data Import Wizard

*.csv files of data, formatted as stated in the wizard dialog, will convert data into CE list variables. Methods in ti_system can then be used to share lists between the emulator CE OS and the Python App. This feature is similar to the Data Import Wizard in TI Connect™ CE.
- If decimal numbers are represented with the use of a comma in the *.csv file, the file will not convert using the Data Import Wizard. Please check your computer operating system number formatting and convert the *.csv to use the decimal point representation. The calculator list and matrix editor use the number format as, for example, 12.34 and not 12,34.