Using Color on the Graph Screen
The examples below show how to set up the graph of a function. Here, the mode is set to FUNCTION and the default settings are assumed.
|
Enter an equation in the Y= editor.
|
|
|||||||||
|
To set the line color in the Y= editor:
|
||||||||||
The spinner dialog displays. Notice the second line in the status bar, which displays hints.
|
|
|||||||||
|
||||||||||
|
Note: The thick line style is the default. It can be changed by pressing | or ~.
|
||||||||||
|
To set a Background Image:
Set GridColor, Axes, and BorderColor as desired.
The spinner menu becomes active. |
|
|||||||||
Note: There are five Image Vars included in your TI-84 Plus CE online calculator. |
||||||||||
Note: You can manipulate the graph to “fit” an object in the Background Image Var. You can also use QuickPlot and Fit Equation to fit an equation to a shape. (See QuickPlot.) |
|
|||||||||