Exam Mode and Exam LED

Use Press-to-Test to manage exams using TI graphing calculators.

The examiner will tell you when to set your calculator in exam mode.

• Press-to-Test is a three-key sequence to place the TI-82 Advanced Edition Python in the allowed state for an exam.
• The Exam LED will blink amber when you have properly set the calculator up for the exam.
• You can create TI-Basic programs during the exam.
• Press-to-Test Mode:
- Deletes all RAM and Archive files with exceptions:
- Retains TI-developed Apps.
- Disables Pics, Images, and Program variables.
- Sets Mode settings to default.

Topic Links

Using Press-to-Test Mode

1. Turn the calculator OFF.
2. Press and hold down the ‘, Í and É keys, and then release.
3. The RESET OPTIONS screen displays.
4. Press OK to first validate any loaded TI Apps and then set up the exam mode. When validation and test mode setup is complete, the confirmation screen will display.

Note: A validation screen may display when entering Exam Mode. Please wait while the files are validated.

5. Press any key to place the calculator in test mode.
6. Exam LED will blink amber.

Note:

• A blue status bar is shown on the TI-82 Advanced Edition Python when in EXAM MODE and EXAM MODE ENABLED.
• All variables, including AppVars, stored in RAM and in archived memory are deleted.
• Pic & Image Vars are disabled.

• In memory management (y L Mem Management/Delete), disabled files will display with the not equal sign.

Bringing a Calculator Out of Exam Mode

You can re-enable all disabled calculator files by using one of the following methods:

• Use TI Connect™ CE Actions > Calculatrices Couleur : quitter le Mode Examen to quit the exam mode on any connected graphing calculator. You may also send a calculator file to the connected graphing calculator to quit from exam mode.
• Link two TI-82 Advanced Edition Python graphing calculators using a unit-to-unit USB cable and then transfer a file by using y 8, ENVOYER RECEVOIR.

To clear a calculator of files created during an exam:

1. Turn off the calculator while in exam mode.
2. "Re-Press-to-Test" - press and hold down the ‘, Í and É keys, and then release.
3. Select OK when you see the Reset Verification Screen. The calculator is now "clean."

Tip: To preserve battery life, quit Exam Mode Press-to-Test after the exam using TI Connect™ CE.