Batteries

The TI-82 Advanced Edition Python graphing calculator comes equipped with:

AAA batteries.
USB computer cable for transferring files

Battery CAUTION

Do not ingest battery, Chemical Burn Hazard
This product contains a coin or button cell battery. If the coin or button cell battery is swallowed, it can cause severe internal burns in just 2 hours and can lead to death.
Keep new and used batteries away from children.
Always completely secure the battery compartment. If the battery compartment does not close securely, stop using the product, remove the batteries, and keep them away from children.
If you think batteries might have been swallowed or placed inside any part of the body, seek immediate medical attention.
Call a local poison control center for treatment information.
Even used batteries may cause severe injury or death.
Non-rechargeable batteries are not to be recharged.
Do not force discharge, recharge, disassemble, heat above 140F (60C) or incinerate. Doing so may result in injury due to venting, leakage or explosion resulting in chemical burns.
Ensure the batteries are installed correctly according to polarity (+ and -).
Do not mix old and new batteries, different brands or types of batteries, such as alkaline, carbon-zinc or rechargeable batteries.
Risk of fire or explosion if battery is replaced by an incorrect type.
Remove and immediately recycle or dispose of batteries from equipment not used for an extended period of time according to local regulations. Do NOT dispose of batteries in household trash or incinerate.

Topic Links