Resetting the Calculator

Resetting the calculator:

Clears the display, all 10 memories, any unfinished calculations, and all worksheet data.
Restores all default settings
Returns operation to the standard-calculator mode

Because the calculator includes alternative methods that let you clear data selectively, use reset carefully to avoid losing data needlessly. (See section “Clearing Calculator Entries and Memories”.)

For example, you might reset the calculator before using it for the first time, when starting a new calculation, or when having difficulty operating the calculator and other possible solutions do not work. (See “In Case of Difficulty”.)

Pressing 2nd Reset ENTER

1. Press & }. The RST ? and ENTER indicators appear.

Note: To cancel reset, press & U. 0.00 appears.

2. Press !. RST and 0.00 appear, confirming that the calculator is reset.

Note: If an error condition exists, press P to clear the display before attempting to reset.

Performing a Hard Reset

You can also reset the calculator by gently inserting a pointed object (such as an unfolded paper clip or similar object) in the hole marked RESET in back of the calculator.