TI Bluetooth® Adapter Update Software

Free Windows computer software to update the Sketch on the TI Bluetooth® Adapter over USB

• Auto-detects the TI Bluetooth® Adapter
- If there are multiple connected adapters, the software will select first device it detects

Steps to update the sketch on the TI Bluetooth® Adapter

1. Download the update software from the TI website at:
education.ti.com/bluetooth
2. Install and launch the software
3. Download the latest sketch from the TI website at:
education.ti.com/bluetooth
4. Connect the TI Bluetooth® Adapter to the PC using a standard A-to-micro-B PC cable
5. The update software will detect the adapter and enable the update button
6. Do not disconnect the TI Bluetooth® Adapter while the update is in progress.
7. The software will inform you once the update is done. You can disconnect the TI Bluetooth® Adapter and connect another one that needs to be updated.