TI-84 Plus CE Graphing Calculator
Familiar TI-84 Plus functionality in a sleek new design that features a crisp color screen
Familiar TI-84 Plus functionality in a sleek new design that features a crisp color screen
Visualize concepts clearly and make faster, stronger connections between equations, data, and graphs in full color.
The TI-84 Plus CE is approved for use on the following exams:
The TI Rechargeable Battery conveniently recharges using a USB cable, wall charger or TI Charging Station CE.
The same menu structure and navigation as the TI-84 Plus family make it easy to pick up and learn.
Easily distinguish classroom calculators from student-owned calculators with EZ-Spot loss prevention features. The “school bus yellow” back cover, and faceplate inscribed “School Property” provide effective theft deterrence.
Subject-specific lessons and tools that help students gain an understanding of math and science concepts. Find activities written for the TI-83 Plus, TI-84 Plus and TI-84 Plus CE.
Webinars, tutorials, workshops and courses delivered by experienced, certified T³ instructors to help you meet your classroom goals. For more than 25 years, the T³ organization has been providing professional development that combines content-rich curriculum, hands-on technology training and compelling instruction on best teaching practices.
*SAT & AP are registered trademarks of the College Board, which was not involved in the production of and does not endorse this product. ACT is a registered trademark of ACT, Inc., which does not endorse this product. Policies subject to change. Visit www.collegeboard.com and www.act.org
{"commands":[{"click":"chrome:field:editcontrol({command:\"webedit:editlink\"})","header":"Edit link","icon":"/temp/iconcache/networkv2/16x16/link_edit.png","disabledIcon":"/temp/link_edit_disabled16x16.png","isDivider":false,"tooltip":"Edits the link destination and appearance","type":""},{"click":"chrome:field:editcontrol({command:\"webedit:clearlink\"})","header":"Clear Link","icon":"/temp/iconcache/networkv2/16x16/link_delete.png","disabledIcon":"/temp/link_delete_disabled16x16.png","isDivider":false,"tooltip":"Clears The Link","type":""},{"click":"chrome:common:edititem({command:\"webedit:open\"})","header":"Edit the related item","icon":"/temp/iconcache/office/16x16/cubes.png","disabledIcon":"/temp/cubes_disabled16x16.png","isDivider":false,"tooltip":"Edit the related item in the Content Editor.","type":"common"},{"click":"chrome:rendering:personalize({command:\"webedit:personalize\"})","header":"Personalize","icon":"/temp/iconcache/office/16x16/users_family.png","disabledIcon":"/temp/users_family_disabled16x16.png","isDivider":false,"tooltip":"Create or edit personalization for this component.","type":"sticky"}],"contextItemUri":"sitecore://master/{4E6F66D3-2830-48DA-9CDD-86411953DD88}?lang=en&ver=1","custom":{},"displayName":"Link","expandedDisplayName":null}
footnote1
Now you can add a new dimension to your students’ learning experience interactive geometry for your calculator. Create excitement in the classroom as you construct, analyze, and transform mathematical models and geometric diagrams.
Cabri Jr. was developed for TI by CabriLog® with renowned French mathematician Jean-Marie Laborde. Just take a look at what Cabri™ Jr. geometry app can do:
Alter geometric objects on the fly to see patterns, make conjectures, and draw conclusions -- and, you'll get a more intuitive and highly interactive interface
Your calculator can become a more versatile tool to use in a variety of classes with the addition of spreadsheet capabilities!
This App will present equations in function, parametric, or polar form and provides a simple way to graph the four conic shapes:
Enter the required parameters to:
Students can enter inequalities using symbols, plot inequalities including union and intersection shades, trace points of interest (intersections) between functions, store (x,y) coordinate pairs for viewing and enter Linear Programming functions
These Apps will translate all prompts, error messages and most functions into French, German, Spanish, Dutch, Swedish and Portuguese
This App is not just your basic periodic table - students can also study and review trends in the periodic table easily with their TI graphing calculator.
Additional benefits include:
Polynomial Root Finder capabilities include:
Simultaneous Equation Solver capabilities include:
Explore probability theory with interactive animation that simulates the rolling of dice, tossing of coins and generating random numbers on your calculator.
Options include:
In addition, students can export data for further exploration.
Science Tools provides the capability to perform unit conversions on your calculator. Get more use from your calculator in the science classroom with this App.
App elements include:
Within seconds, educators can gain control over testing environments using TI TestGuard™ to
Students can visually draw conclusions about functions and improve graphing comprehension with this App. To take advantage of this App's capabilities, simply input functions, and view changes in the function as the parameters are changed.
Students can:
The EasyData® App from Vernier Software & Technology is simple data collection software for the TI-84 Plus CE. Explore the world around you using this App. The EasyData® App auto-launches data collection when used with Vernier EasyTemp® sensor, and loads built-in experiments for every supported Vernier sensor. EasyData® supports data collection with Vernier USB sensors (TI-84 Plus family only), CBR™ 2, using the TI-84 Plus CE.
Extend the power of your graphing calculator and create a customizable approach to learning with accessories for the TI-84 Plus CE graphing calculator.
The TI Charging Station CE, designed for the TI-84 Plus CE graphing calculator, keeps calculators organized.
Key Features:
Included with Teacher Pack purchases and also available separately as a standalone purchase.
This simple software complements the TI-84 Plus family of graphing calculators, letting the educator project a representation of the calculator’s display to the entire class. It is an ideal demonstration tool for leading classroom instruction of math and science concepts.
TI Connect™ CE computer software allows for connectivity between your computer and graphing calculator. Transfer data, update your Operating System (OS), download Calculator Software Applications (Apps), edit and load programs to your graphing calculator.
The CBR 2™ motion sensor, which connects directly to your graphing calculator, is designed for teachers who want their students to collect and analyze real-world motion data, such as distance, velocity and acceleration. Great for algebra through calculus and statistics, physical science and physics.
The TI-84 Plus CE graphing calculator comes with a TI Rechargeable Battery.
For students, the TI Rechargeable Battery is expected to last up to two weeks of normal use on a single charge. For classroom use, the TI Rechargeable Battery is expected to last up to five days of normal use on a single charge. Use the USB cable or the TI-Power Adapter (included) to power up the handheld.
Students graph a quadratic function and investigate its symmetry by choosing pairs of points with the same y-value.
Learn MoreStudents represent and analyze mathematical situations and structures using algebraic symbols.
Learn MoreStudents use a simulation to find the experimental probability of independent events.
Learn MoreStudents are to find the solution to a system of linear equations using technology. They are presented with two problems; music sales and parking lot fees.
Learn MoreTI has partnered with Atomic Learning to develop informative, step-by-step videos that drill down into the TI-84 Plus CE graphing calculator’s capabilities.
Learn More