Education Technology

Solution 34412: Evaluating Composite Functions for a Specific Value of X on the TI-84 Plus C Silver Edition Graphing Calculator.

How can I evaluate the composition of two functions given a specific x-value on the TI-84 Plus C Silver Edition graphing calculator?

In order to evaluate the composition of two functions, given a specific value of x, refer to the following example.

Example: Find the composition of the following two functions when x = .5
f(x) = x2 + 3x - 2
g(x) = 2x + 3

Please Note: Many textbooks indicate function compositions using the notation f(g(x)) or (f ° g)(x).

Solution:

Let Y1 = f(x) and Y2 = g(x)

1) Press [Y=] to go to the Y= Editor screen.
2) Input x2 + 3x - 2 into the Y1 slot, then press [ENTER].
3) Input 2x + 3 into the Y2 slot, then press [ENTER].
4) Press [VARS] [Þ] [1] to select 1:Function from the Y-VARS menu.
5) Press [1]  to select 1:Y1 then press [(].
6) Press [VARS] [Þ] [1] to select 1:Function from the Y-VARS menu again.
7) Press [2]  to select 2:Y2 then press [)] [ENTER].

Please Note: The Y3 slot should read Y3 = Y1(Y2

8) Press [Ü] [Ý] [Ý] [Ý] to select the '=' to the right of Y1, then press [ENTER] to disable the function from being graphed. The black square surrounding the '=' disappears once the function is disabled.
9) Press [ß] [ENTER] to disable the Y2 function from being graphed as well.

 

10) Press [GRAPH] to graph the composite function
11) Press [TRACE] then input .5 and press [ENTER]

 

The coordinates are displayed, even if CoordOff format is selected.  The y-value of 26 is the solution to the problem.

For additional instructions on evaluating functions and performing other calculations, refer to the online guidebooks for your calculator model.