Education Technology

Perimeter of Australia

Published on 10/19/2012

Activity Overview

Students plot points on a map of Australia drawn on the Cartesian plane. The coordinates of the points are used to determine the distance between successive points and the progressive distance (perimeter) of Australia.

Objectives

National Curriculum:
(ACMNA214) Find the distance between two points located on a Cartesian plane using a range of strategies, including graphing software.
Elaborations:
Investigating graphical and algebraically, techniques for finding distance between two points and using Pythagoras' theorem to calculate distance between two points.

Vocabulary

Pythagoras, distance between two points, Cartesian plane, coordinate geometry

About the Lesson

Students plot points on the graph, TI-nspire determines the coordinates. The formula for the distance between two points is written on the screen. Students connect the appropriate coordinates to the formula and the answer is computed. In their written notes students do the same providing for both technology support and independent determination of the distance between two points.