TI-Nspire™ CX Navigator™ System


Frequently Asked Questions
Where is the TI-Nspire CX Navigator system available for purchase?
The TI-Nspire CX Navigator system is available for purchase from Instructional Product Dealers in the US and Canada.

What is the difference between TI-Nspire CX Navigator system and TI-Nspire Navigator system?
The TI-Nspire CX Navigator includes TI-Nspire CX Wireless Network Adapters which only work with the TI-Nspire CX and TI-Nspire CX CAS handhelds. The TI-Nspire Navigator includes TI-Nspire Navigator Cradles which work with all TI-Nspire handhelds including TI-Nspire, TI-Nspire CAS, TI-Nspire CX and TI-Nspire CX CAS handhelds. Both systems include TI-Nspire Navigator Teacher Software that works with either system.

Can I use a mix of any TI-Nspire handheld simultaneously with a single TI-Nspire CX Navigator System?
Yes, the TI-Nspire Navigator System can support a mix of TI-Nspire, TI-Nspire CAS, TI-Nspire CX and TI-Nspire CX CAS handhelds with either the TI-Nspire Navigator Cradles or TI-Nspire CX Wireless Network Adapters.

Can I use TI-Nspire CX Wireless Network Adapters and TI-Nspire Navigator Cradles on the same TI-Nspire Navigator System?
Yes, but please keep in mind that the TI-Nspire CX Wireless Network Adapter is only compatible with TI-Nspire CX and TI-Nspire CX CAS handhelds.

Which TI graphing calculators are compatible with the TI-Nspire CX Navigator system?
The TI-Nspire CX Navigator system supports any combination of the TI-Nspire handhelds. This includes the TI-Nspire CX, TI-Nspire CX CAS, TI-Nspire, and TI-Nspire CAS handhelds. Please keep in mind that the TI-Nspire and TI-Nspire CAS will only work with the TI-Nspire Navigator Cradles and not the TI-Nspire CX Wireless Network Adapters.

What are the TI-Nspire Navigator System Requirements?
Please click here for the system requirements.

I followed all the steps, but my TI-Nspire CX Wireless Network Adapters will not connect. What do I do?
Make sure you update your TI-Nspire handhelds with the latest operating system. Updates are available in the Download Center. You may also try to manually add the cradles by going to Tools > Network Manager > Add Wireless Client(s). Additionally, make sure each handheld has selected the class network by pressing HOME>: 5: Settings > 6: Network.

Can I get more information about the TI-Nspire Navigator system at Teachers Teaching with Technology™ (T3™) conferences?
The T³ International Conference and T³ Regional Conferences are excellent opportunities for learning more about the TI-Nspire Navigator system.

Will there be professional development available for TI-Nspire Navigator system?
TI-Nspire Navigator system is integrated in to all T³ Professional Development.

Will TI-Nspire Navigator system work with the TI-84 keypad snapped in?
No. When the TI-84 Plus keypad is snapped into the TI-Nspire handheld, the TI-Nspire handheld works just like a TI-84 Plus calculator, and therefore the handhelds cannot be used with the TI-Nspire Navigator system. However, they can be used with the TI-Navigator system.

How do I get technical support for the TI-Nspire Navigator system?
Trained TI-Nspire Navigator system specialists are available by email ti-navigator@ti.com, online chat, or by phone at 1-866-TI-NAVIGATOR (1-866-846-2844) and select Option 1, or by completing an interest form.

How can I find out more about the TI- Nspire Navigator system?
Call 1-866-TI-NAVIGATOR (1-866-846-2844) and select Option 2 to speak to a TI-Navigator product specialist, email ti-navigator@ti.com or complete an interest form.

Where can I find information about the wireless technology used in the TI-Nspire Navigator System?
Information regarding the wireless technology used in the TI-Nspire Navigator System is in the technical white paper by visiting education.ti.com/navigator/whitepaper. Feel free to share with your IT Administrator.

What is the wireless technology used in the TI-Nspire CX Navigator classroom system?
The TI-Nspire CX Navigator classroom system uses WiFi wireless technology to connect the TI-Nspire handhelds to the access point. This is the same technology used in home wireless routers and other electronic devices like laptops and smartphones.
Where to Buy