Rocket Simulation Activity -- Exploring Quadratic Functions
Rocket Simulation Activity -- Exploring Quadratic Functions
Students will model projectile motion in both function and parametric graphing. This was designed as an in-class modeling activity to be used prior to actually launching air-powered projectile rockets.
A set of data is given in a spreadsheet and students create model functions using a variety of methods: vertex form (then using grab and move to fit the curve to the data points), standard form (using matrices), and quadratic regression.
This investigation usually follows the study of quadratic functions. The quadratic function is characterized by a parabolic curve, by viewing the scatter plot, we can see it will open downward. The data represents a rocket path, height per unit of time; the symmetry of the curve is obvious. The vertex will represent the height the rocket attained in t seconds. The activity includes parametric graphing, as previously pointed out. The teacher will determine the appropriateness of this activity for classes he/she instructs.
The teacher should review the various forms of a quadratic function and also methods used to create the model function in the different forms. The teacher should also review parametric graphing and any formulas that are necessary for the students to complete this activity successfully.
This activity is designed to be student-centered. The teacher may act as a facilitator while students work independently or cooperatively. The teacher will inform students in which manner they are to work.
The ready-to-use worksheet will provide a written assignment which can be used for daily credit points.
The file titled rocketsimSOL shows the expected results of working through the activity and the screenshots are included in the step-by-step instructions.
Possible Extensions:
The actual outdoor launch activity consisted of a vertical launch to determine initial velocity, horizontal launch at different angles, launching at angles with altimeter measurement to create right triangle trigonometry and a probability launch activity.

Before the Activity Files
During the Activity Files
Vernier EasyData,Vernier EasyLink and Vernier EasyTemp are registered trademarks of Vernier Science Education.