Extended Law of Sines
College
Extended Law of Sines
This activity is to be used with pre-service mathematics teachers, in-service teachers in a project of professional development or high school students of Geometry. The main goal is to demonstrate how to use the TI-nspire technology to enhance the students capacity to elaborate and demonstrate conjectures.
The relationship between the lengths of the sides of a triangle inscribed in a circle, the Sine of the internal angles and the radius of the circle is studied.
Install the file ExtendedLawofSines.tns in all the TI-handhelds. Students must have copy of the document LES-students.pdf or LES-students.doc. Students must be divided in groups of three.
Students will discuss with their group mates if they have previously heard about the Extended Law of Sines. If it is so, they will try to remember the statement and will write it on the space that is provided.
All students will turn to the page that contains the statement of the Law. After moving the vertices of the triangle on the circumference and seeing the different representations of the Extended Law of Sines they will verify that it holds, making the appropriate measurements as indicated (page 8). The demonstration of the Law is based on two theorems that have been seen previously:
1) The angle inscribed in a semicircle is a right angle.
2) Given B and C, two fixed points on a circle, for two points A and J on the circle
The professor must ask if this proof holds for all the cases and he (she) must observe that it is also necessary to prove that the Law holds in the case
Prove that:
1. the perpendicular bisectors of the sides of a triangle concur at a point
2. the point of concurrence of the perpendicular bisectors of the sides of a triangle is the center of the circle circumscribed to the triangle.
Additional Files
College
Vernier EasyData,Vernier EasyLink and Vernier EasyTemp are registered trademarks of Vernier Science Education.