which calc is right for me

Back to Help with TI-Nspire

Notes templates

The Notes application provides templates for creating three types of notes:

  • Q&A for questions and answers, with the answer shown or hidden

  • Proof for an outline structure containing statements and reasons

  • Default for open-formatted text entry

Applying a Notes template

  1. While in the Notes work area, press to display the Notes menu.

  2. On the Templates menu, select the specific template to apply.

Using the Q&A Template

Use the Q&A template to create questions and answers. You have the option to show or hide the answer, so you can create questions for review and hide the answers. When you use the document as a study aid, you can verify that your answers are correct.

Press to move the text cursor between the Question and Answer areas of the template.

Using the Proof Template

The proof template provides an outline structure for statements and corresponding reasons.

Press to move the text cursor between the Statements and Reasons areas of the template.

Back to Help with TI-Nspire