which calc is right for me

Back to Help with TI-Nspire

Filling adjacent cells

You can repeat a cell's formula or value throughout adjacent cells. This gives you a quick way to fill cells with the same value or create a series of cells that contain the same formula. You can fill down within a column. To do this:

  1. Select the cell whose value or formula you want to repeat.

  2. Press menu to display the Lists & Spreadsheet menu.

  3. On the Data menu, select Fill Down.

  4. Press repeatedly to move down, selecting the range of cells that will hold the repetitions.

  5. Press enter.

The selected cell is duplicated throughout the selected range. Please note:

  • In step 1, you can select more than one cell to be repeated.

    If you do, make sure that you select enough destination cells to hold the repeated copies.

  • If you select multiple cells in step 1 and the cells contain a simple sequence (such as 1,2,3 or 5,10,15,20), the sequence is continued in the filled area.



Follow along with this example for filling adjacent cells:

  1. To create a 10 item list of numbers increasing by 5 starting at 0, type 0 into cell a1 and type "= a2 + 5" into cell a2 and press enter.



  2. Select cell a2.

  3. Press menu to display the Lists & Spreadsheet menu.

  4. On the Data menu, select Fill Down.

  5. Click a2 and scroll down to a10.



Back to Help with TI-Nspire