Back to Help with TI-Nspire
Changing the page layout
When you create a new document in your TI-Nspire™ handheld, it contains space to add one application. If you need to add more than one application to a page, you can change the layout to accommodate as many as four applications.
You can choose a standard layout, provided as a menu item, or you can customize a layout to suit your needs.
Choosing a standard layout
- Press
to display layout options.
- If you want to select a standard layout, press
.
- Press the number that corresponds to the layout you want to apply to the page.
For example, press
to create a two-pane layout, divided vertically on the page. The page is divided into the layout design you have selected.
- Press
to move to the right pane on the page.
- Press the number of the application you want to add the new pane.
For example, to add the Graphs & Geometry application to the right pane, press
.
Creating a custom layout
If the standard layouts do not meet your needs, you can customize the space allotted to applications on a page.
- Press
to display layout options.
- Press
to select the custom split option.
The standard layout displays, with a blinking divider between the application panes.
- Press
,
,
or
to move the divider to adjust the height and width of the panes in the layout. Note: Press
or
to select a defined layout.
- Press
or
to accept the layout dimensions.