Back to Help with TI-Nspire
Keypad changing and battery replacement
Your TI-Nspire™ handheld operates in two modes:
- TI-Nspire
- TI-84 Plus Silver Edition
Dual Keypads
Your TI-Nspire handheld works with two keypads: the first is the TI-Nspire keypad and the second is the TI-84 Plus keypad.
TI-84 Plus keypad (on left) and TI-Nspire keypad (attached to handheld)
Changing the keypad
Caution: When changing keypads, be certain that the handheld is completely powered down before removing the keypad. Removing the keypad before the display clears may result in loss of data.
-
Remove the cover, and turn the handheld over. Slide the latch release to the right.
The keypad releases.
-
Turn the handheld right side up, and slide the keypad away from the display screen.
-
Lift the keypad off the handheld.
-
Insert the other keypad.
Ensure that it fits comfortably into the guides on the bottom and sides of the handheld.
Note: The keypad does not slide in from the bottom edge of the unit. Instead, fit it into the guides just above the batteries.
-
When the keypad is properly seated on the handheld, push the keypad toward the display screen.
The keypad clicks into place when properly seated and completely inserted into the handheld.
The TI-Nspire math and science learning handheld uses four AAA batteries that are provided with the product.
Replacing batteries
Caution: When removing the keypad to change batteries, be certain that the handheld is completely powered down. Removing the keypad before the display is cleared may result in loss of data.
- Remove the keypad from the handheld.
-
Carefully remove the batteries.
Caution: You may need to use a tool to remove the batteries as they fit tightly in the unit. If you use a tool, be careful not to damage either the batteries or the handheld.
-
Insert fresh batteries.
Ensure that the + side of each battery faces away from the display screen.
- Replace the keypad.
Battery Precautions
Take these precautions when replacing batteries:
- Do not leave batteries within the reach of children.
- Do not mix new and used batteries. Do not mix brands, or types within brands, of batteries.
- Do not mix rechargeable and non-rechargeable batteries.
- Install batteries according to polarity (+ and -) diagrams.
- Do not place non-rechargeable batteries in a battery recharger.
- Properly dispose of used batteries immediately.
- Do not incinerate or dismantle batteries.
- Seek medical advice immediately if a cell or battery has been swallowed.
Additional precautions for rechargeable batteries:
- Use only the charger recommended for the cell or battery, or the one that was provided with the original equipment.
- Remove the cell or battery from the charger or alternating current adapter when not in use or being charged.
- Use of the battery in other devices may result in personal injury or damage to equipment or property.
For proper disposal of used batteries:
Do not mutilate, puncture, or dispose of batteries in fire. The batteries can burst or explode, releasing hazardous chemicals. Discard used batteries according to local regulations.