Graphing Calculators
-
TI-Nspire™ CX Handheld
You can color-code equations, objects, points and lines on the full-color, backlit display. Purchase the TI-Nspire CX CAS handheld and TI-Nspire Student Software together.
-
TI-Nspire™ CX CAS Handheld
Calculate in style - with a high-resolution, full-color display that makes it easy to see every exponent, variable and line. Purchase the TI-Nspire CX CAS handheld and TI-Nspire Student Software together.
-
TI-Nspire™ handheld with Touchpad
3-in-1 value! Handheld, full-color student software and TI-84 Plus Keypad all in one package. The handheld is permitted on SAT*, AP*, ACT**, IB®**, PSAT/NSMQT** and Praxis™ exams, and many state tests.
-
TI-Nspire CAS handheld with Touchpad
2-in-1 value! Handheld with built-in Computer Algebra System and full-color student software in one package. The handheld is permitted on SAT*, AP*, PSAT/NSMQT** and Praxis™ exams, and many state tests.
-
TI-84 Plus Silver Edition graphing calculator
Nine times the memory, twice the speed of TI-83 Plus model. Enter math as it appears in textbooks. USB cable included. Periodic Table and Organizer Applications preloaded.
-
TI-84 Plus graphing calculator
Three times the memory, twice the speed of TI-83 Plus model. Enter math exactly as it appears in textbooks. USB cable included.
-
TI-83 Plus graphing calculator
Easy to use for math and science. FLASH™ ROM memory to update and add Applications. Compatible with TI-84 Plus family, which offers greater memory and speed.
-
TI-73 Explorer™ graphing calculator
For grades 6-8. Designed with features to explore fractions all the way through pre-algebra topics. The next step up from 2-line and 4-line scientific calculators.
-
TI-89 Titanium graphing calculator
Computer Algebra System (CAS) functionality and 3D graphing for AP*, advanced mathematics and engineering courses.
Scientific Calculators
-
TI-30 Xa scientific calculator
Convert fractions and decimals, degrees, radians and grads and more. You can also perform basic scientific and trigonometric functions.
-
TI-30X IIS scientific calculator
The two-line display scientific calculator combines statistics and advanced scientific functions and is a durable and affordable calculator for the classroom.
-
TI-36X Pro™ scientific calculator
TI's latest and most advanced scientific calculator features a high-quality MultiView™ display and MathPrint™ capability. Ideal for computer science and engineering courses.
-
TI-34 MultiView™ scientific calculator
View multiple calculations on a 4-line display and scroll through entries. See math symbols, including stacked fractions, exactly as they appear in textbooks.
-
TI-30XS MultiView™ scientific calculator
Navigate menus similar to a graphing calculator. Enter multiple calculations and compare results on the same screen. Do fractions as they appear in textbooks.
*SAT & AP are registered trademarks of the College Entrance Examination Board, which was not involved in the production of and does not endorse this product.
**PSAT/NMSQT/SAT/Advanced Placement Program/AP/College Board are registered trademarks of the College Entrance Examination Board, which was not involved in the production or development of TI products. ACT is a registered trademark of ACT, Inc., which does not endorse this product. IB is a registered trademark of the International Baccalaureate Organization. Praxis is a trademark of the Educational Testing Service.