You are here: Working with TI‑Nspire™ Documents > Working with Applications

Working with Applications

When you first open a new document or add a new problem to a document, you select an application from a menu.

The following illustration shows how a document containing the Lists & Spreadsheet application appears in the work area.

À

Document name. Tabs show the names of open documents. Click a name to make it the active document.

Á

Page Size. Shows the document's page size as Handheld or Computer. You can use the TI‑Nspire™ File menu to convert a document from one page size to the other.

Â

Problem/Page counter. Labels the problem number and page number of the active page. For example, a label of 1.2 identifies Problem 1, Page 2.

Ã

Settings. Double-click to view or change the Document Settings for the active document or to change the default Document Settings.

Ä

Angle Mode. Shows an abbreviation of the angle mode (Degrees, Radians, or Gradians) in effect. Hover the pointer over the indicator to see the full name.

Å

Zoom. Enabled in Handheld preview only (click Document Preview on the toolbar and select Handheld). Click and select a magnification value, or click the zoom-to-fit button to make the preview adapt automatically to window size.

Æ

Boldness. Enabled in Computer preview only (click Document Preview on the toolbar and select Computer). Click and select a value to increase or decrease the boldness of text and other items.

Working with Multiple Applications on a Page

You can add up to four applications to a page. When you have multiple applications on a page, the menu for the active application is displayed in the Documents Toolbox. Using multiple applications involves two steps:

Changing the page layout to accommodate multiple applications.
Adding the applications.

You can add multiple applications to a page even if an application is already active.

ClosedAdding Multiple Applications to a Page
ClosedSwapping Applications

 

© 2006 - 2015 Texas Instruments Incorporated