You are here: Graphs Application > Zooming/Rescaling the Graphs Work Area

Zooming/Rescaling the Graphs Work Area

Rescaling in the Graphs application affects only the graphs, plots, and objects that reside in the Graphing view. It has no effect on objects in the underlying Plane Geometry view.

Rescaling by Dragging Along an Axis

To rescale the x and y axes proportionally, drag a tic mark on either axis.
To rescale only one axis, hold down Shift and drag a tic mark on the axis.

Zooming Using a Zoom Tool

From the Window / Zoom menu, select one of the tools.
- Zoom - Box (Click two corners of a box to define the area to show.)
- Zoom - In
- Zoom - Out

Zooming to Predefined Settings

From the Window / Zoom menu, select one of the predefined Zoom settings.
- Zoom - Standard
- Zoom - Quadrant 1
- Zoom - Standard User
- Zoom - Standard Trig
- Zoom - Standard Data
- Zoom - Fit

Entering Custom Window Settings

1. From the Window / Zoom menu, select Window Settings.
2. Enter a value for each setting. You can use expressions for exact input, as shown below.

  

On TI‑Nspire™ products, fractional input is preserved as-is. Other exact inputs are replaced with the evaluated result.

 

  

On TI‑Nspire™ CAS products, fractional and other exact inputs are preserved.

 

© 2006 - 2015 Texas Instruments Incorporated