You are here: Graphs Application > Measuring Objects

Measuring Objects

Measurement values update automatically as you manipulate the measured object.

Note: Measurements of objects created in the Graphs application are displayed in generic units named u. Measurements of objects created in the Geometry application are displayed in centimeters (cm).

ClosedMeasuring Length of a Segment, Circle Arc, or Vector
ClosedMeasuring Distance Between Two Points, a Point and a Line, or a Point and a Circle
ClosedMeasuring Circumference of a Circle or Ellipse or the Perimeter of a Polygon, Rectangle, or Triangle
ClosedMeasuring a Side of a Triangle, Rectangle, or Polygon
ClosedMeasuring Area of a Circle, Ellipse, Polygon, Rectangle, or Triangle
ClosedMeasuring Slope of a Line, Ray, Segment, or Vector
ClosedMeasuring Angles
ClosedMeasuring Angles using the Directed Angle Tool
ClosedMoving a Measured Value
ClosedEditing a Measured Length
ClosedStoring a Measured Value as a Variable
ClosedLinking a Measured Length to an Existing Variable
ClosedDeleting a Measurement
ClosedLocking or Unlocking a Measurement

 

© 2006 - 2015 Texas Instruments Incorporated