You are here: Graphs Application > Creating Shapes Using Gestures (Math Draw)

Creating Shapes Using Gestures (Math Draw)

The Math Draw tool lets you use touchscreen or mouse gestures to create points, lines, circles, and other shapes.

Math Draw is available in:

Geometry view without the analytic window displayed.
Graphing view when the x scale and y scale are identical. This avoids non-circular ellipses and non-square rectangles appearing as circles and squares.

Math Draw is not available in the 3D Graphing view or in the Geometry view with the analytic window displayed.

Activating Math Draw

1. If using the Geometry view with the analytic window visible, use the View menu to hide the window.
2. On the Actions menu, select Math Draw.

The Math Draw icon appears. You can begin using the tool.

Canceling Math Draw

When you have finished using the Math Draw tool, press Esc.

The tool also closes if you select a different tool or change views.

ClosedCreating Points
ClosedDrawing Lines and Segments
ClosedDrawing Circles and Ellipses
ClosedDrawing Triangles
ClosedDrawing Rectangles and Squares
ClosedDrawing Polygons
ClosedUsing Math Draw to Create Equations
ClosedUsing Math Draw to Measure an Angle
ClosedUsing Math Draw to Find a Mid-point
ClosedUsing Math Draw to Erase

 

© 2006 - 2015 Texas Instruments Incorporated