Previous TopicNext Topic
You are here: Welcome to the TI‑Nspire™ App for iPad® > Using Variables > Creating a Variable from a Geometry Value

Creating a Variable from a Geometry Value

In this example, the area of the triangle will be the value for a variable named "triangle."

1. Tap the value you want to store to select it, and then tap it again to open the context menu.

2. Tap Store.

var := appears before the selected value. This is the default name.

.

3. Replace the default name var with the variable name you want to give the value.
4. Tap ENTER.

The value is saved to that variable name, and the stored value or its name appears in bold text to indicate that it is a stored value.

 

© 2013 Texas Instruments Incorporated