Previous TopicNext Topic
You are here: Welcome to the TI‑Nspire™ App for iPad® > Working with Documents > Changing Document Settings

Changing Document Settings

Document settings control how all numbers, including elements or matrices and lists, are displayed in TI‑Nspire™ documents. You can change the default settings at any time, and you can specify settings for a specific document.

Complete the following steps to customize the settings that are applied to your document.

1. Create a new document or open an existing document.
2. Tap Settings .

When you open Document Settings the first time, the default settings are displayed.

3. Tap the menu name to open the menu and view the available values for each setting.

.

Field

Value

Display Digits

Float
Float1 - Float12
Fix0 - Fix12

Angle

Radian
Degree
Gradian

Exponential Format

Normal
Scientific
Engineering

Real or Complex Format

Real
Rectangular
Polar

Calculation Mode

Auto
CAS: Exact
Approximate

Note: Auto mode shows an answer that is not a whole number as a fraction except when a decimal is used in the problem. Exact mode (CAS) shows an answer that is not a whole number as a fraction or in symbolic form, except when a decimal is used in the problem.

Vector Format

Rectangular
Cylindrical
Spherical

Base

Decimal
Hex
Binary

Unit System (CAS)

SI
Eng/U.S.
4. Select the desired settings.
5. Choose one of the following options:
To apply the customized settings to ALL documents, tap Make Default.
To apply the settings to the open document only, tap Done.
To restore default settings, tap Restore.

 

© 2013 Texas Instruments Incorporated