Previous TopicNext Topic
You are here: Welcome to the TI‑Nspire™ App for iPad® > Data & Statistics Application > Working with Plots

Working with Plots

Dot Plots
Dot plots are also known as frequency plots, and represent one-variable numerical data.
Dot plots are the default plot type for numerical data.
One dot represents each value in the list.
Each dot is displayed on the axis at a point that corresponds to the value.
Box Plots
Box plots are used to plot one-variable numerical data in a modified box.
"Whiskers" extend from each end of the box.
Box plots are used to compare two or more sets of data that use the same scale.
Histograms
A histogram plots one-variable numerical data and depicts the distribution of data.
The number of bins displayed depends on the number of data points and how the points are distributed.
A value that occurs on the edge of a bin is counted in the bin to its right.
Normal Probability Plots

Shows one set of numerical data against the corresponding quartile (z) of the standard normal distribution.

Scatter Plots
Shows the relationship between two sets of numerical data.
You also plot a scatter plot using the Quick Graph tool in the Lists & Spreadsheet application.
X-Y Line Plots
This plot is a type of scatter plot in which data points are plotted and connected in order of appearance in the two variables.
An X-Y line plot depicts the relationship between two sets of data.
The left-most column of data is represented on the horizontal axis.
Exploring and Analyzing Plotted Data
Drag a point to move it. As you move a point, the values associated with the point change in the work area and in the list of variables.
To change a variable on an axis, tap the Add Variable region, and then tap another variable name.
From the Tools menu:
- Tap Plot Type to select another supported plot type.
- Tap Plot Properties to clear all variables or to modify properties such as add and remove X and Y variables, add a summary list, or force a categorical X.
- Tap Actions to insert text or sliders. You can also select all points in the plot.
- Tap Analyze to choose analysis options such as add a moveable line, plot a value or function, or activate the Graph Trace tool.

 

© 2013 Texas Instruments Incorporated