Module 22 - Power Series
 
  Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test
 
 Introduction
 

In this module you will learn to represent power series algebraically and graphically. The graphical representation of power series can be used to illustrate the amazing concept that certain power series converge to well known functions on certain intervals. In the first lesson you will start with a power series and determine the function represented by the series. In the last two lessons you will begin with a function and find its power series representation.


Lesson Index:

    22.1 - Power Series

    22.2 - Maclaurin Series

    22.3 - Taylor Series

After completing this module, you should be able to do the following:

  • Define and graph the sequence of partial sums for a power series
  • Illustrate the interval of convergence for a power series
  • Differentiate and integrate a power series to obtain other power series
  • Use the taylor( command on the TI-89 to generate Maclaurin and Taylor Series for a given function

Next >
  ©Copyright 2007 All rights reserved. | Trademarks | Privacy Policy | Link Policy