| Module 16 - The Fundamental Theorem | ||||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test | ||||||||||
| Lesson 16.3: The Fundamental Theorem of Calculus | ||||||||||
|
A restatement of the Fundamental Theorem of Calculus is presented in this lesson along with a corollary that is used to find the value of a definite integral analytically. Restating the Fundamental Theorem You have discovered the Fundamental Theorem in the context of finding areas under a curve but a more general version of this theorem can be proved without an appeal to area. The following is a restatement of the Fundamental Theorem. If f is continuous on [a, b], then the function
has a derivative at every point in [a, b], and the derivative is
That is, the derivative of a definite integral of f whose upper limit is the variable x and whose lower limit is the constant a equals the function f evaluated at x. This is true regardless of the value of the lower limit a. The function named F is the same as the area function that was previously explored. Using the Restated Fundamental Theorem
16.3.1 Use the restatement of the Fundament theorem to evaluate the following derivatives, then check your predictions with the TI-89. Click here for the answer. 16.3.2 Predict the following derivative. Check your answer with the TI-89. Hint: You will have to use the chain rule.
Click here for the answer. 16.3.3 Evaluate the following derivative and check with your TI-89.
Click here for the answer. 16.3.4 Find a more general version of the Fundamental theorem by predicting the following derivative. Check your work with the TI-89.
Click here for the answer. Using a Corollary of the Fundamental Theorem The following corollary of the Fundamental theorem gives a method for evaluating a definite integral. Corollary If f is continuous on [a,b], then
The function F is called an antiderivative of the function f.
16.3.5 Use the corollary to predict the value of
Click here for the answer.
16.3.6 Use the corollary of the Fundamental theorem to evaluate
Click here for the answer.
|
||||||||||
| < Back | Next > | ||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|
||||||||||