Module 15 - Answers
 
Lesson 1
 
 Answer 1
 
15.1.1  

Rectangle x-coordinate y-coordinate Width Height Area
1 1/4 1/16 1/4 1/16 1/64
2 1/2 1/4 1/4 1/4 1/16
3 3/4 9/16 1/4 9/16 9/64
4 1 1 1/4 1 1/4
Total         15/32

 
 Answer 2
 
15.1.2  

 
 Answer 3
 
15.1.3  

We can read that

 
Lesson 2
 
 Answer 1
 
15.2.1

The area under f(x) = x2 and above the x-axis between x = 0 and x = 1 is square unit.

 
 Answer 2
 
15.2.2 The function f(x) = 2x + 1 should be entered into y1 before the program is executed and the Viewing Window should be adjusted to include the interval [0, 3]. The graph below is shown in the window [0, 3] x [0, 10].

The graph illustrating the midpoint rectangles is at left below and the approximate areas found using different types of rectangles is shown at right.

 

 
Lesson 3
 
 Answer 1
 
15.3.1

In the screen shown, the value of was found by two methods using the definite integral key. In the first, the function g was defined and then the definite integral was evaluated with its name. In the second, the expression that defines the function was entered directly. In both cases, the area under the graph of g(x) = 2x + 1 and above the x-axis between x = 0 and x = 3 is 12 square units.

 
 Answer 2
 
15.3.2

The area under the curve g(x) = 2x + 1 between x = 0 and x = 3 is 12.

 
Self Test
 
 Answer 1
 

0.3025

 
 Answer 2
 

0.2025

 
 Answer 3
 
 
 Answer 4
 
 
 Answer 5
 
 
 Answer 6
 
 

  ©Copyright 2007 All rights reserved. | Trademarks | Privacy Policy | Link Policy