Module 6 - Answers
 
Lesson 1
 
 Answer 1
 
6.1.1   Evaluate and f(0).

It may be faster to copy and paste the previous commands from the History Window to the Edit Line and change to 0.

Although exists, f(0) is undefined. Therefore, is not continuous at x = 0.

 
Lesson 2
 
 Answer 1
 
6.2.1 From the graph, it appears and , which suggests an infinite discontinuity.

 
Lesson 3
 
 Answer 1
 
6.3.1 The left- and right-hand limits are and .

The function will be continuous if these limits are equal. Setting 2 + k = 5 gives k = 3. So if k = 3, and the function is continuous.

 
 Answer 2
 
6.3.2 The function will be discontinuous at x = 2. The parabolic piece of the graph will be shifted up so that it does not connect with the linear piece.
 
 Answer 3
 
6.3.3

 
Self Test
 
 Answer 1
 
II and III
 
 Answer 2
 
A removable discontinuity (hole) can be seen at at x = –1

The window shown is [–7.9, 7.9] x [–3.8, 3.8] (ZoomDec) with xres = 1.

 
 Answer 3
 
k = 0
 
 Answer 4
 

The window shown is [–7.9, 7.9] x [–3.8, 3.8] (ZoomDec)

 
 Answer 5
 
 

  ©Copyright 2007 All rights reserved. | Trademarks | Privacy Policy | Link Policy