Module 27 - Answers
 
Lesson 1
 
 Answer 1
 
27.1.1   The other possible coordinates are , where k is any integer, or , where k is any odd integer.
 
 Answer 2
 
27.1.2  

The polar point has approximate rectangular coordinates (1, 1.7321).

 
Lesson 2
 
 Answer 1
 
27.2.1

The graph is a three leafed rose.

 
 Answer 2
 
27.2.2  

When n is even there are 2n leaves. When n is odd there are n leaves.

 
 Answer 3
 
27.2.3  

The graph has six overlapping leaves.

 
 Answer 4
 
27.2.4  

a = b gives a cardioid.

The graph shown is r = 2 + 2cos .

gives a limaçon with an inner loop.

The graph shown is r = 1 + 2 cos( ).

gives a dimpled limaçon.

The graph shown is r = 3 + 2 cos( ).

gives a convex limaçon.

 
Lesson 3
 
 Answer 1
 
27.3.1 The area is approximately 12.5664 square units. Because the function r = 2 represents all points that are 2 units away from the origin, the graph is a circle of radius 2 units centered at the origin. Its exact area is A = (2)2 = 4 square units, which agrees with the area found.
 
 Answer 2
 
27.3.2 The area inside the circle and outside the cardioid is square units.
 
Self Test
 
 Answer 1
 

The point (r, ) = (5.385, 1.951) in polar coordinates is the same as the rectangular point (-2, 5).

 
 Answer 2
 
The point (x, y) = (1.618, 1.176) in rectangular coordinates is the same as the polar point .
 
 Answer 3
 

 
 Answer 4
 
The slope of the tangent line to r = 2 - 3 cos at = / 4 is approximately 0.892.
 
 Answer 5
 
The area of one leaf is about 4.189 square units.
 
 

  ©Copyright 2007 All rights reserved. | Trademarks | Privacy Policy | Link Policy