Module 25 - Answers
 
Lesson 1
 
 Answer 1
 
25.1.1   The arches of the cycloid are higher and wider.
 
 Answer 2
 
25.1.2   The radius of the tire is a units.
 
 Answer 3
 
25.1.3  

After 7 revolutions the reflector appears to return to its starting point.

 
Lesson 2
 
 Answer 1
 
25.2.1 

At t = 0.5

dy/dt 1.2984

and

dx/dt 0.6225.

These values satisfy the Chain Rule since , which is the previously found value for dy/dx.

 
 Answer 2
 
25.2.2  

 

The line tangent to the curve when t = 2 is y = 0.6421(x - 1.0907) + 1.4161.

 
Lesson 3
 
 Answer 1
 
25.3.1 The arc length for is about 1.5 units.
 
 Answer 2
 
25.3.2   The length of the spiral of Archimedes between t = 0 and t = 10 is about 51.748 units.
 
Self Test
 
 Answer 1
 
 
 Answer 2
 
 
 Answer 3
 
 
 Answer 4
 
The tangent line to the curve at is y = 0.5(x + 0.5) - 0.5.
 
 Answer 5
 
The length of the curve between t = 0 and is about 3.341 units.
 
 

  ©Copyright 2007 All rights reserved. | Trademarks | Privacy Policy | Link Policy