Module 19 - Answers
 
Lesson 1
 
 Answer 1
 
19.1.1  

 
 Answer 2
 
19.1.2  
[0, 4, 1] x [-5, 15, 1]
The net area is 4 square units.
 
 Answer 3
 
19.1.3  

The graph shown below is an approximation of the net-area function.

 
Lesson 2
 
 Answer 1
 
19.2.1

The total area bounded by y = x3 – 3x2x + 3 and the x-axis on the interval [0, 4] is 12 square units.

 
 Answer 2
 
19.2.2

The x-coordinate of the right point of intersection is approximately 1.562.

 
 Answer 3
 
19.2.3  

The area between the two curves is approximately 11.682 square units.

 
Lesson 3
 
 Answer 1
 
19.3.1

The length of the curve y = x2 between x = -1 and x = 2 is approximately 6.126 units.

 
Self Test
 
 Answer 1
 
The net area bounded by f(x) = x3 - 4x2 - 4x + 16 and the x-axis is approximately 19.583 square units.
 
 Answer 2
 

The screen below shows one possible net-area function for f(x) = x3 - 4x2 - 4x + 16 over [0, 5].

 
 Answer 3
 
The total area bounded by f(x) = x3 – 4x2 – 4x + 16 and the x-axis over [0, 5] is approximately 32.917 square units.
 
 Answer 4
 
The area between the two curves f(x) = x2 - 1 and g(x) = x is approximately 1.863 square units.
 
 Answer 5
 
The length of the curve f(x) = sin x between x = 0 and x = 2 is approximately 7.640 units.
 
 Answer 6
 
The integral gives the length of f(x) = tanx between x = 0 and x = /4.
 
 

  ©Copyright 2007 All rights reserved. | Trademarks | Privacy Policy | Link Policy