| Module 13 - Extreme Values of Functions | ||||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Lesson 4 | Self-Test | ||||||||||
| Lesson 13.4: TI-83 Minimum and Maximum Features | ||||||||||
|
The TI-83 has features in the CALCULATE menu that find maximums and minimums. In this lesson you will use these features and compare results with local extrema found in previous lessons. Although these features are usually quite accurate, you should remember they give numerical approximations, not exact values. Miminum and Maximum Features In Lesson 13.2 and Lesson 13.3 you found local extrema of f(x) = x3 - 2x - 2cosx using first and second derivatives. The Minimum and Maximum features in the CALCULATE menu can also be used to approximate the local extrema.
Use the calculator's Minimum feature to approximate the coordinates of the local minimum shown on the graph.
The calculator returns to the graph and prompts you for a left bound.
The calculator now prompts you for a right bound.
The calculator prompts you for an initial guess for the minimum.
The calculator improves on the initial guess and returns an approximation of the coordinates of the local minimum point: (0.559, -2.639). The coordinates of the local minimum are very close to those found in previous lessons. The Maximum feature of the CALCULATE menu can be used to find a local maximum using a similar procedure. 13.4.1 Use the Maximum feature and the procedure described above to find the coordinates of the local maximum of f(x) = x shown in the graph above. Click here for the answer. Approximating Another Minimum Value This last example is a reminder that minimum and maximum values produced by a calculator are not exact. Use the calculator's Minimum feature to approximate the minimum of f(x) = x2.
The calculator provides approximations that are given in exponential notation, and although these approximations are quite close, they are not exact. (Your calculator may provide slightly different values.) The exact coordinates of the minimum point of this parabola are (0,0).
|
||||||||||
| < Back | Next > | ||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|
||||||||||