Module 10 - Answers
 
Lesson 1
 
 Answer 1
 
10.1.1

The slopes of the secant lines appear to converge to 1, so the derivative is probably about 1.

 
Lesson 2
 
 Answer 1
 
10.2.1

appears to be differentiable at x = 0 because it is locally linear there
appears not to be locally there.

 
Lesson 3
 
 Answer 1
 
10.3.1 The derivatives of the function at the given x-values are -4, -2, 0, 2, and 4, respectively.
 
 
 Answer 2
 
10.3.2 The derivative at x = 1.22 is 2.44, which means that the slope of the line tangent to the curve at x = 1.22 is 2.44.
 
 
 Answer 3
 
10.3.3

 

The derivative function is f ' (x) = 6x + 4.

 
 
Self Test
 
 Answer 1
 

6.03, 6.003, 6.0003

 
 Answer 2
 

6

 
 Answer 3
 
6
 
 Answer 4
 

y = 6(x - 1) + 3

[0.9812, 1.0188] x [2.89999, 3.09999]

 
 Answer 5
 

 
 Answer 6
 

y = 6x

 

  ©Copyright 2007 All rights reserved. | Trademarks | Privacy Policy | Link Policy