Module 4 - Answers |
Lesson 1 |
Answer 1 |
4.1.1
The points are only evaluated and plotted for values of t greater than or equal to zero. Because x = t, only values of x that are greater than or equal to zero will be graphed. |
Answer 2 |
4.1.2
The inverse of the parabola is a parabola that is symmetric with respect to the x-axis and is the reflected image of the original parabola across the line y = x. The original parabola and its inverse relation, the thicker graph, are shown below in a [-3,3] x [-3, 3] window. |
Answer 3 |
4.1.3
The graphs of y = (x - 3)2 and it's inverse are reflections of one another across the line y = x. The thicker graph below is the graph of y = (x - 3)2, the thinner graph is the graph of its inverse relation, and the dotted line is y = x. The inverse relation is not a function. |
Lesson 2 |
Answer 1 |
4.2.1
The graph is a circle of radius one centered at the origin. |
Answer 2 |
4.2.2
Points being plotted simultaneously on both the unit circle and the sine wave have the same y-values. |
Answer 3 |
4.2.3
The graph of y = -3sin(2(x + 1)) - 4 is the graph of y = sin x that has been:
Reflected across the x-axis. Compressed Horizontally by a factor of 1/2, that is, the new period is .
Horizontally shifted left 1. |
Lesson 3 |
Answer 1 |
4.3.1
The new graph would have a smaller period so the peaks would be closer together. |
Self Test |
Answer 1 |
The cosine function is defined parametrically as X1T = T, Y1T = cos(T), and its inverse is defined as X2T = cos(T), Y2T = T. |
Answer 2 |
Windows may vary.
The window shown is [-2 , 2 , 0.2] x [-2 , 2 , /2] x [-4, 4, 1]. |
Answer 3 |
Windows may vary.
The window shown is [0, , 0.1] x [-4.5, 4.5, 1] x [-2, 4, 1] |
Answer 4 |
The transformed graph is the graph of y = sin x that has been
Reflected over the x-axis Vertical stretched by a factor of 2 (amplitude = 2) Horizontal shrunk by a factor of , making the period 4 Horizontal shifted right 3 Vertical shifted up 1
The window shown was determined by selecting 7:ZTrig in the ZOOM menu. The dotted line is y = 1 and the cursor indicates a shift up 1 and right 3 from the origin. |
Answer 5 |
|
Answer 6 |
The frequency is approximately 750/(2
), which is about 119.4 cycles per second.
|
©Copyright 2007 All rights reserved. | Trademarks | Privacy Policy | Link Policy |